This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are having an outside vendor up-screen the part at -55 degrees C. This part is not rated to our test temperature of -55C. The process is they install the IC into a board using a TSSOP socket and check the output voltage at ambient. They ramp the temperature to -55 degrees C and power the part and check the output voltage to see if it's within 5 % of its output. In this case 6.3 volts so anything below 5.850 volts they fail. The concern is besides handling is this or could it cause the part to fail prematurely?
LM2651MTCX-ADJ/NOPB
Hi David,
Absolute junction temperature is -40C. -55C is lower than ABS minimum value. The device is not guaranteed to work normally under such temperature.
BRs
Zixu