This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53679: Compensation parameters

Part Number: TPS53679

Hi, 

I am using TPS53679 and CSD95490 combination for generating 0.8V for 83A and 1.2V for 46A. I have used 4 phases of CSD95490 for 0.8V and 2 phases for 1.2V. 

I am observing that 0.8V is going down due to glitches when it goes below 0.776mV, which is the minimum limit. 

I guess the parameters for the transient response for the voltages are not okay.

We are not able to find any help with these parameters in the documents.

Can you please help how to find these parameters? 

AC_GAIN, AC_LL, INT_Time, INTGAIN and Ramp voltage? Should we keep the USR2 and USR1 switched off?

Also, please help on what to enter for BLANK_TIME_RISING and MINTOFF parameters?

What to enter for PS_APH? Should it be "One phase active in ps1 mode" or "Two phase active"?

Regards,

Rasif