This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A84: Do we have low iq LDO with SNS?

Part Number: TPS7A84

Hi Teams,

My customer is using TPS7A84 which has Remote sns for ATE application. But the Iq of TPS7A84 is 2.8mA, which is too large for the system. Do we have low iq LDO parts to meet this requirement?

BRs,

Marsh

  • Hello Marsh,

    Unfortunately, currently we don't have any recommended devices with lower Iq in the same current space. In the high current space, our recommended devices have Iq starting at 2.8-mA. Is there a particular reason why customer needs low Iq for a 3A LDO? Also, is 3A(high current), SNS pin and low Iq needed?

    Best,

    Eunize Tobias