This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I have a query need your help.
After learning cycle, the FCC updated and larger than design capacity.
but the SOH is only 99%. Why the SOH doesn't reach 100%? The design capacity is 4750mAh. After learning cycle is completed, Qmax has been updated and the FCC updated to 4850mAh.
Load selection 3
Load mode 1
Waiting for your reply.
Thanks
Star
Hi Anthony
Thanks for your reply.
SOH FCC update is only 4735mAh. FCC was 4816mAh during discharge and updated to 4766mAh after 5 hours of rest. Qmax parameter updated to 5187mAh.
Please help check it.
Thanks
Star
Hi Star,
Can you please tell me which firmware version is being used for this bq40z50?
Regards,
Anthony Baldino