Part Number: BQ40Z50
The customer need to use BQ40z50 to drive 4 LED to display the RSOC.
The function requirement is as below.

Could you pls provide the recommending Hard Circuit design and the related parameter configuration?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Fabio,
There is an FAQ page on how to configure the gauge for lower LED counts than 5, you can use the EVM schematic as a guide for the hardware configuration, just remove the 5th LED. We do not support LED blinking at very low SOC, we can support mid-point blinking which gives better resolution, the only other option we would have is LEDRCA which will cause the LEDs to flash when RCA is set.
Sincerely,
Wyatt Keller