Other Parts Discussed in Thread: BQ25756, TIDA-010208
Hello,
I am planning to design a BMS using the BQ76952 and BQ25756. (See design overview in picture below) The battery charger should also be integrated on the BMS board and communicate with the same MCU (host) as the monitor. In the data sheets it is recommended to connect the ground of the monitor via a net tie to the battery.
The question is if the bq25756 charger is on the same board and communicates with the same microcontroller, which ground should it be connected to? VSS or PGND? If it is connected to PGND, the shunt can cause small voltage differences between the MCU and BQ25756 (I2C bus and other signal lines between host and charger)
The same question arises for the MCU. In the datasheet of the BQ76952 the MCU is connected to PGND (see picture below). In the TIDA-010208 reference design, the MCU is connected to VSS. (See picture below)
The communication to the outside world will be isolated
What would you recommend for the GND connections?
Thank you in advance
Lukas
Datasheet: