Part Number: BQ76952
Other Parts Discussed in Thread: BQ7718, BQ77216, BQ34Z100-R2, BQ78350-R1A, BQ34Z100
I noticed in the BQ76952, there is built in cell over/under voltage Protection. But on the Eval board, there are separate BQ771807 cell over/under protection devices. This seems redundant. But it seems as of the BQ771807 autonomously asserts the Fuse (if installed) as well as the Red LED. If not using the Fuse, then it really only turns on the RED LED. From reading the data sheet of the BQ76952, it seems as if I can configure each cell COV and CUV levels and have them interrupt using the Alert pin.
What is TI's recommendation for using the BQ771807?
I also read in the forums that the BQ76952 does not support gauging but it does have a coulomb counter. I was assuming the coulomb counter will provide capacity of the battery based on current flow via the sense resistor. Is this a correct assumption?
Thanks!