This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22677: Dual LM22677 self-synchronise not working as expected

Part Number: LM22677

On a development board, I have two LM22677 buck converters for two different voltage levels (adjustable at 12V, fixed at 5V). As per the datasheet section 7.3.4, the RT/SYNC pins of the two connectors are pulled low with 1k resistors and tied together with a 2N7002 N-channel MOSFET, Q1. Please note I accidentally routed the enable pins (7) to input power. On the actual board, those pins are bent up and soldered together with a jumper.

The datasheet then specifies: The two regulators will be clocked at the same frequency but slightly phase shifted according to the minimum off-time of the regulator with the fastest internal oscillator. The slight phase shift helps to reduce stress on the input capacitors of the regulator.

Therefore, I would expect that probing the SW pins of each converter would show a phase shift of the minimum off-time, around 200 ns. However, the actual scope shows that the two waveforms are exactly in phase.

Would I not expect to see a 200 ns phase shift? Am I misunderstanding the datasheet or have I designed the circuit incorrectly?

  • Hi Arjun,

    Can you zoom in the area of the rising edge and see the phase shift? As the phase shift is very slight, your waveform looks good to me.

    Regards,

    Hongjia