Other Parts Discussed in Thread: LMR36506
Hello,
We are using 2 of the LV2862 with a similar design as in datasheet.
One of them converts 48V to 24V and the other one converts the 24V to 5V. The maximum load current connected to a conductivity sensor is 20mA. The issue with the current switching regulator is that it is always in the ECO mode and the sawtooth signal creates a noise in the output which is not desirable. Is there anyway that we could use the same switching regulator and get rid of the ECO mode. ( I added some resistors in the output to increase the load current and could get out of the ECO mode but that is not desired and we do not want to waste the current that way). If not what would be your suggestion for our specific application which works at low currents?
Best Regards,
Shirin Toloue