Other Parts Discussed in Thread: LMR36006,
Hi,
I would like to use the Y version as a power source to my circuit (input voltage could be from 9-36V) with the following conditions:
- Over sleep mode - the DC-DC should supply power of 20-30uA /7V.
- Over power mode - the DC-DC should supply power of 50mA/7V,
- Can these two options work?
- Do I need to calculate the inductor value only according to the 50mA load?
- what is the minimum current the DC-DC can supply?
Thank you,