This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMQ66430-Q1: [Compal]Schematic review

Part Number: LMQ66430-Q1
Other Parts Discussed in Thread: LMQ66430, LMQ66420

Hi Expert,

Could you help to review the schematic for LMQ66430-Q1?

1.LMQ66430

輸入電壓Vin 12V

輸出電壓Vout 3.6V

Choke 2.2uH (Isat 5A)

power budget  2A

 2.LMQ66430

輸入電壓Vin 12V

輸出電壓 Vout 3.3V

Choke 2.2uH(Isat 5A)

power budget  2.5A

3.LMQ66430

輸入電壓12V

輸出電壓1.1V

Choke 2.2uH(Isat 5A)

power budget  2.3A

TI_LMQ66430_LMQ66420_1.8V_1.2V_1.1V_FAE_0131.pdfTI_LMQ66430_3.6V_3.3V_FAE_0131.pdf

Far