Other Parts Discussed in Thread: TPSM83100, TPS631000
Hello,
We have used the Part#TPS63802DLAR in my design and prepare the schematic, Layout.
We have also used the Web Bench to design the hardware. Attached is the web bench generated data and below is the design requirement.
Requirement: -
Input voltage: 1.3V to 3.6V
Output voltage: 5V.
Output current: 500mA-750mA.
We are facing two different issues during board bring up.
Problem 1: -
After receiving the board, at the time of board bring up, the design is giving output 5V when the input voltage is 1.72V, If i decrease the Input voltage below the 1.7V the output become 0V.
Problem 2: -
When Input is 1.72V and Output is 5V at that time If I connect a load of 10OHms to set the load current of 500mA, the output voltage will decrease to 3.23V and this time Input is taken 1.002A current (set current is 2A).
Try solution.
1) Removed the EN pin resistor divider and directly connect EN pin to VIN.
Kindly review the attached Web Bench reference schematic and also attached the actual design Image for your review.
Please provide the solution at earliest.
Thanks,