This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25982: Is this Part TPS259827ONRGET will work with Load Condition?

Part Number: TPS25982

Hi,

We are going to use this eFuse in power side in our design with load condition. I need to know the fuse will work or not. 

If the part will not work with load condition means, please recommend alternate part for our condition. 

Input = 12V/7.5A