Hello All,
I have used efuse TPS259827ONRGET in my project for protecting the sensor power from short circuit.
But i have facing an issue with the efuse (TPS259827ONRGET).
I have Configured the load switch in following configuration :
1. Current limit for 11..2A (Rlim = 130E ).
2. Itimer Capacitor 47nF used (22mSec).
3. Slew rate dv/dt capacitor = 8.2nF
I have tested with the Automotive DC bulb (12V/Watts) for the load test.
When the load switch is turned on I didn't get the voltage at the output (12V)and also didn't get the power good fault.
Kindly let me know your valuable comments.
Thanks and Regards,
Mohamed Sidiq.H