HI
We are using the battery charger BQ25720RSNR in laptop project. We are using three cell battery. We are facing issue with this battery charger.
When we insert the DC jack (J17) and turn on the charger the battery charger is working fine and generating the output. But when we do multiple cycles of on and off of battery charger the battery charger stops generating the output. We checked the DC jack input power. It is coming proper 19.5V input but not generating the system power.
We have also attached the battery charger schematic for your reference. We have checked the voltage at C385 (VCC_CHGR_EMI_VIN_R) it is coming but we are not able to get any voltage at TP164 (VCC_VBATA).
We have also checked the signals (BC_HS_DRV1, BC_LS_DRV1) which is driving the dual mosfet (Q14 and Q15), It is low. When this issue is not come and battery charger is generating the output properly at that time these signals are at 5V level.
Kindly check and help to resolve this issue.