Hi,
Related E2E case: (TPS546D24A: Noisy VR, need to verify design and hw/sw configuration, link: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1305420/tps546d24a-noisy-vr-need-to-verify-design-and-hw-sw-configuration)
We are using the TPS546 on a PCB design involving low voltage and high current.*
Vin=5V
Vout,nom=300mV
Imax~35A*
*design is for high current, although in this test we only pull lower current, Imax ~3A.
Purpose of experiment:
Understand PCB noise which seems to originate from the TPS546 and is observed on other power rails.
Test environment:
- Tektronix MSO64B oscilloscope with TPP1000 probe (<4pF C), and using barrel-tip measurement.
- Test PCB “SUT” (system under test), which is composed of
- (a) the “OVR” On-board VR, TPS546 installed to supply the “VDD” main rail,
- Fsw = 1.1 MHz
- Compensation hex value: 0x137C420884
- #Used TI calculator, PhMa:83, AvMa:-13
- (b) other voltage sources (discussed as needed below), and
- (c) multiple IC components acting generally as a “resistive load”
- (a) the “OVR” On-board VR, TPS546 installed to supply the “VDD” main rail,
- External “EVM” - the TPS546D24AEVM-2PH from TI
- Fsw = 550 kHz, 2 Phase operated in 1 Phase mode.
- Compensation hex value: 0x1220C62246
- 5V PSU - Power supply is a Siglent SPD3303X-E (3 Ch, 3.2A per Ch)
- Keithley Benchtop DMM, for measuring voltages independently
Variable 1: TPS546 - we have two VRs under test within the same system.
In the first set of experiments, we use the “OVR” (on-board VR).
In the second set of experiments, we used the “EVM”. In this experiment, we disable the OVR by lifting the output inductor pad, and instead inject power from the EVM, connected through low resistance banana cables.
Variable 2: Observing the voltages with “VDD OFF” vs “VDD ON” (Note, 5V is present on the PCB in all of these captures. This variable just turns the TPS546 off and on)
We captures these signals on the four scope channels (e.g. “C1” means channel 1):
C1=5V=Yellow
C2=0p9V=Blue
C3=3v3=Red
C4=VDD=Green
Measurement method: for each power rail, we used a tip and barrel measurement across a capacitor near the load. For VDD, we measured at a bulk capacitor near the output inductor.
Results:
Experiment 1a, OVR - VDD OFF
Some noise on 3.3V, no exact signature detected. No noise above 50mV. No noise spikes observed.
Experiment 1b, OVR - VDD ON
Above shows 1.1 MHz switching noise on VDD and coupled noise on other power rails. Noise is above 100mVp-p.
Above shows 1.1 MHz switching noise as observed on 3.3V rail (898ns == 1.1MHz) Noise is above 100mVp-p.
Experiment 2a, EVM - VDD OFF
Some noise on 5V, 0.9V, and 3.3V, no exact signature detected. No noise above 50mV. No noise spikes observed.
Experiment 2b, EVM - VDD ON
1.1MHz** switching noise observed on VDD, up to 270mVp-p. **Note the 2-PH EVM is operating in 1 Phase mode at a reported 550kHz, so we see overlapping switching signals detected. Other rails observe some of the switching noise, but amplitude is less.
Summary:
- Switching noise evident from both OVR and EVM.
- OVR noise is strongly coupled into other power rails.
- EVM is weakly coupled into other power rails.
Sidenote: We have Cout (output capacitance) in the same amount and size as provided by the TI Webench, 6x100uF and 5x560uF.
Questions for TI:
- Is noise of this magnitude from the EVM expected, 100mV spikes measured near the load?
- How can we reduce noise?
- Request: Design review (confidential, need to email/meet separately).
Thanks,
Tom