This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3481: Performance Review

Part Number: LM3481

Hi team. I've been working on the LM3481 SEPIC converter for a while now and it alwyas keeps on comin up with newer problems.

Vin:18V to 30V
Vout:24V/1A

A coupled inductor design is being used and the DRQ125-220-R is being used as the inductor. All the values of caps and resistors being used are as recommended by the Webench Design for these parameters staed above and i use a fsw of 520kHz for my application. 
During testing yesterday, the borad was mounted along with a heatsink on the inductor, mosfet and diode to make it cool and test was being carried out at 0.5A continuos. The output voltage lost regulation after a while and shot up to about 100V (timestamp:2/10/2024 12:39:55 PM ) at the output. This happened for the first time and kept happening a few times. Attaching the test report here for review. I can send you the schematic and PCB on pricate chats for review but i am not able to figure out why this keeps happening. Please advice.

2/10/2024 12:39:26 PM	24.414V	0.0000A
2/10/2024 12:39:27 PM	24.415V	0.0000A
2/10/2024 12:39:27 PM	24.410V	0.0000A
2/10/2024 12:39:28 PM	24.408V	0.0000A
2/10/2024 12:39:28 PM	24.409V	0.0000A
2/10/2024 12:39:29 PM	24.407V	0.0000A
2/10/2024 12:39:29 PM	24.404V	0.0000A
2/10/2024 12:39:30 PM	24.403V	0.0000A
2/10/2024 12:39:30 PM	24.405V	0.0000A
2/10/2024 12:39:31 PM	1.1253V	0.0000A
2/10/2024 12:39:32 PM	1.0918V	0.2875A
2/10/2024 12:39:32 PM	1.1116V	0.2893A
2/10/2024 12:39:33 PM	24.420V	0.2862A
2/10/2024 12:39:33 PM	24.449V	0.4986A
2/10/2024 12:39:34 PM	24.499V	0.4986A
2/10/2024 12:39:34 PM	24.567V	0.4986A
2/10/2024 12:39:35 PM	24.582V	0.4986A
2/10/2024 12:39:35 PM	24.588V	0.4986A
2/10/2024 12:39:36 PM	24.593V	0.4986A
2/10/2024 12:39:36 PM	24.597V	0.4986A
2/10/2024 12:39:37 PM	24.595V	0.4986A
2/10/2024 12:39:38 PM	24.593V	0.4986A
2/10/2024 12:39:38 PM	24.591V	0.4986A
2/10/2024 12:39:39 PM	24.590V	0.4986A
2/10/2024 12:39:39 PM	24.591V	0.4986A
2/10/2024 12:39:40 PM	24.587V	0.4986A
2/10/2024 12:39:40 PM	24.584V	0.4986A
2/10/2024 12:39:41 PM	24.583V	0.4986A
2/10/2024 12:39:41 PM	24.583V	0.4986A
2/10/2024 12:39:42 PM	24.587V	0.4986A
2/10/2024 12:39:42 PM	24.587V	0.4986A
2/10/2024 12:39:43 PM	24.581V	0.4986A
2/10/2024 12:39:43 PM	24.572V	0.4986A
2/10/2024 12:39:44 PM	24.569V	0.4986A
2/10/2024 12:39:44 PM	24.568V	0.4986A
2/10/2024 12:39:45 PM	24.571V	0.4986A
2/10/2024 12:39:45 PM	24.569V	0.4986A
2/10/2024 12:39:46 PM	24.572V	0.4986A
2/10/2024 12:39:46 PM	24.581V	0.4986A
2/10/2024 12:39:47 PM	24.585V	0.4986A
2/10/2024 12:39:48 PM	24.587V	0.4986A
2/10/2024 12:39:48 PM	24.584V	0.4986A
2/10/2024 12:39:49 PM	24.615V	0.4986A
2/10/2024 12:39:49 PM	24.645V	0.4988A
2/10/2024 12:39:50 PM	24.653V	0.4986A
2/10/2024 12:39:50 PM	24.662V	0.4986A
2/10/2024 12:39:51 PM	24.699V	0.4986A
2/10/2024 12:39:51 PM	24.801V	0.4986A
2/10/2024 12:39:52 PM	26.585V	0.4986A
2/10/2024 12:39:52 PM	26.585V	0.4986A
2/10/2024 12:39:53 PM	26.585V	0.4986A
2/10/2024 12:39:53 PM	26.585V	0.4986A
2/10/2024 12:39:54 PM	26.585V	0.4986A
2/10/2024 12:39:54 PM	36.361V	0.4986A
2/10/2024 12:39:55 PM	36.361V	0.4986A
2/10/2024 12:39:55 PM	104.53V	0.0000A
2/10/2024 12:39:56 PM	99.575V	0.0000A
2/10/2024 12:39:56 PM	97.491V	0.0000A
2/10/2024 12:39:57 PM	30.138V	0.0000A
2/10/2024 12:39:58 PM	22.330V	0.0000A
2/10/2024 12:39:58 PM	12.924V	0.0000A
2/10/2024 12:39:59 PM	5.5436V	0.0000A
2/10/2024 12:39:59 PM	4.2647V	0.0000A
2/10/2024 12:40:00 PM	3.3554V	0.0000A
2/10/2024 12:40:00 PM	2.6785V	0.0000A
2/10/2024 12:40:01 PM	1.7490V	0.0000A
2/10/2024 12:40:01 PM	1.4227V	0.0000A
2/10/2024 12:40:02 PM	1.1597V	0.0000A
2/10/2024 12:40:02 PM	0.7724V	0.0000A
2/10/2024 12:40:03 PM	0.6300V	0.0000A
2/10/2024 12:40:03 PM	0.5133V	0.0000A
2/10/2024 12:40:04 PM	0.3382V	0.0000A
2/10/2024 12:40:04 PM	0.2732V	0.0000A
2/10/2024 12:40:05 PM	0.2195V	0.0000A
2/10/2024 12:40:05 PM	0.1753V	0.0000A
2/10/2024 12:40:06 PM	0.1086V	0.0000A
2/10/2024 12:40:07 PM	0.0839V	0.0000A
2/10/2024 12:40:07 PM	0.0639V	0.0000A
2/10/2024 12:40:08 PM	0.0362V	0.0000A
2/10/2024 12:40:08 PM	0.0275V	0.0000A
2/10/2024 12:40:09 PM	0.0214V	0.0000A
2/10/2024 12:40:09 PM	0.0142V	0.0000A
2/10/2024 12:40:10 PM	0.0122V	0.0000A
2/10/2024 12:40:10 PM	0.0109V	0.0000A
2/10/2024 12:40:11 PM	0.0095V	0.0000A
2/10/2024 12:40:11 PM	0.0083V	0.0000A
2/10/2024 12:40:12 PM	0.0079V	0.0000A
2/10/2024 12:40:12 PM	0.0077V	0.0000A
2/10/2024 12:40:13 PM	0.0070V	0.0000A
2/10/2024 12:40:13 PM	0.0067V	0.0000A
2/10/2024 12:40:14 PM	0.0064V	0.0000A
2/10/2024 12:40:14 PM	0.0061V	0.0000A
2/10/2024 12:40:15 PM	0.0059V	0.0000A
2/10/2024 12:40:16 PM	0.0058V	0.0000A
2/10/2024 12:40:16 PM	0.0056V	0.0000A
2/10/2024 12:40:17 PM	0.0053V	0.0000A
2/10/2024 12:40:17 PM	0.0053V	0.0000A
2/10/2024 12:40:18 PM	0.0052V	0.0000A
2/10/2024 12:40:18 PM	0.0050V	0.0000A
2/10/2024 12:40:19 PM	0.0049V	0.0000A
2/10/2024 12:40:19 PM	0.0049V	0.0000A
2/10/2024 12:40:20 PM	0.0046V	0.0000A
2/10/2024 12:40:20 PM	0.0046V	0.0000A
2/10/2024 12:40:21 PM	0.0044V	0.0000A
2/10/2024 12:40:21 PM	0.0037V	0.0000A
2/10/2024 12:40:22 PM	0.0038V	0.0000A
2/10/2024 12:40:22 PM	0.0040V	0.0000A
2/10/2024 12:40:23 PM	0.0040V	0.0000A
2/10/2024 12:40:23 PM	0.0040V	0.0000A
2/10/2024 12:40:24 PM	0.0040V	0.0000A
2/10/2024 12:40:24 PM	0.0038V	0.0000A
2/10/2024 12:40:25 PM	0.0037V	0.0000A
2/10/2024 12:40:26 PM	0.0037V	0.0000A
2/10/2024 12:40:26 PM	0.0037V	0.0000A
2/10/2024 12:40:27 PM	0.0035V	0.0000A
2/10/2024 12:40:27 PM	0.0035V	0.0000A
2/10/2024 12:40:28 PM	0.0034V	0.0000A
2/10/2024 12:40:28 PM	0.0032V	0.0000A
2/10/2024 12:40:29 PM	0.0032V	0.0000A
2/10/2024 12:40:29 PM	0.0031V	0.0000A
2/10/2024 12:40:30 PM	0.0031V	0.0000A
2/10/2024 12:40:30 PM	0.0029V	0.0000A
2/10/2024 12:40:31 PM	0.0029V	0.0000A
2/10/2024 12:40:31 PM	0.0029V	0.0000A
2/10/2024 12:40:32 PM	0.0029V	0.0000A
2/10/2024 12:40:32 PM	0.0028V	0.0000A
2/10/2024 12:40:33 PM	0.0028V	0.0000A
2/10/2024 12:40:33 PM	0.0028V	0.0000A
2/10/2024 12:40:34 PM	0.0028V	0.0000A
2/10/2024 12:40:35 PM	0.0026V	0.0000A
2/10/2024 12:40:35 PM	0.0026V	0.0000A
2/10/2024 12:40:36 PM	0.0026V	0.0000A
2/10/2024 12:40:36 PM	0.0026V	0.0000A
2/10/2024 12:40:37 PM	0.0026V	0.0000A
2/10/2024 12:40:37 PM	0.0026V	0.0000A
2/10/2024 12:40:38 PM	0.0025V	0.0000A
2/10/2024 12:40:38 PM	0.0025V	0.0000A
2/10/2024 12:40:39 PM	0.0025V	0.0000A


I have not been able to get the board to keep working reliably for the specs that i've mentioned above. Please do review my files and let me know if there is some underlying major issue that i might be missing.

Thanks and Regards
Noel