Other Parts Discussed in Thread: LM5148
Hi,
I design a board based on LM25148. I also got PCB review for it.
Now i am testing the board.
I noticed that as i increase the load current, the input voltage at converter start dropping drastically so the output voltages..
The board is designed to output 7.4V and minimum input voltages will be 8.4V.
In the given data, the input supply is setup at 8.4V on supply and 1st column show the voltages measure at input terminals of the converter.
Input Voltages V (drop shown at Meter) | Output Voltages V | Load current A |
8.4 | 7.39 | 0 |
7.7 | 7.38 | 2 |
6.9 | 6.79 | 4 |
6.2 | 5.95 | 6 |
If i increase the power supply voltages to maintain input voltages at 8.4V then it give desire output. Now the question is why input voltages are dropping? As input voltage drop so obviously output will be less than input.