Part Number: TCA8418
Hi,
I am designed a custom PCB and I am facing a very small issue related to program if someone can help me with it. It is Arduino Code. I know it is out of your jurisdiction but I think someone can help me with it because I also found Arduino code example in other thread provided by TI guy.
I have a keypad as shown in below picture.
I am getting some different number on each key press . I don't mind if i can get a unique number of each key. The rest i can mange.
I received number like that
21 to 30 for SW1 to SW10
11 to 20 for SW11 to SW20
For SW21 to SW29 , I received pair number.
For example
SW21 >> 1 & 2
SW22 >> 2 & 3
SW23 >> 3 & 4
.
.
SW29 >> 9 & 10
SW30 >> 10 only.
I have two request if you can help me with it.
- Assign number in same sequence for SW1 to SW10 as for SW11 to SW20. For example, instead of 21 to SW1, it should be 1 for SW1. The sequence of SW11 to SW20 is perfect.
- Assign a single unique number from SW21 to SW30 instead of double number
Serial Monitor DATA
21,22,23,23,23,24,25,26,27,27,28,29,30
11,12,13,14,15,16,17,18,19,20
1,2,2,3,3,4,4,5,5,6,6,7,7,8,8,9,9,10,10
/* * TCA8418 Driver * This code is adapted from the phishman's driver for arduino, https://github.com/phishman/TCA8418 * The difference is that it is written to be easily ported to another microcontroller * Author: Henry Troutman */ /* * Keyboard PCB Hookup Guide: * 1 -> 3.3V * 2 -> GND * 3 -> SDA * 4 -> SCL * 5 -> INT_PIN * 6 -> RTC_INT (ds3231) */ // Arduino I2C Library #include <Wire.h> // keyboard Constants #define KEYBOARD_ADDRESS 0x34 #define KEYBOARD_INT_PIN 1 #define KEYBOARD_STATE_REGISTER 0x04 #define KEYBOARD_FLAG_REGISTER 0x02 #define KEYBOARD_KEY_DOWN 0x80 #define KEYBOARD_KEY_MASK 0x7F // configuration commands (configures the 3x10 matrix as inputs with pullups, interrupts ... // For more information look at the code in the repo linked above const uint8_t KEYBOARD_CONFIG_COMMANDS[] = {0x1D,0x07,0x1E,0xFF,0x1F,0x03,0x01,0xB9,0x02,0x0F}; // Define our functions before use void keyboard_configure(void); void keyboard_clearFlag(void); uint8_t keyboard_getState(void); // keyInt allows our event to ultimately be handled in the loop volatile bool keyInt = false; void setup() { Serial.begin(9600); Wire.begin(); keyboard_configure(); pinMode(KEYBOARD_INT_PIN,INPUT); // There is an external pullup on the pin // Set up a falling edge pin interrupt on pin 2 attachInterrupt(digitalPinToInterrupt(KEYBOARD_INT_PIN), keyboard_ISR, FALLING); } void loop() { if(keyInt){ uint8_t key_code = keyboard_getState(); // Get first keycode from FIFO if(key_code & KEYBOARD_KEY_DOWN) { // This is where we can write to a screen or handle control keys Serial.print(key_code&KEYBOARD_KEY_MASK); // print the keycode Serial.print(","); keyInt = false; keyboard_clearFlag(); } delay(100); } } void keyboard_configure(void){ for(uint8_t i = 0;i < 9;i+=2){ Wire.beginTransmission(KEYBOARD_ADDRESS); Wire.write(KEYBOARD_CONFIG_COMMANDS[i]); Wire.write(KEYBOARD_CONFIG_COMMANDS[i+1]); Wire.endTransmission(); } } uint8_t keyboard_getState(void){ uint8_t key; Wire.beginTransmission(KEYBOARD_ADDRESS); Wire.write(KEYBOARD_STATE_REGISTER); Wire.endTransmission(); Wire.requestFrom(KEYBOARD_ADDRESS, 1); // request 1 bytes from slave device 0x34 while (Wire.available()) { // slave may send less than requested key = Wire.read(); // receive a byte as character } return key; } void keyboard_clearFlag(void){ Wire.beginTransmission(KEYBOARD_ADDRESS); Wire.write(KEYBOARD_FLAG_REGISTER); Wire.write(0x0F); Wire.endTransmission(); } void keyboard_ISR(void){ keyInt = true; } /* I2C Command Summary Setup board (5x10 keypad) write to Register, value 0x1D, 0x1F 0x1E, 0xFF 0x1F, 0x03 0x01, 0xB9 To get keys read 1 byte from 0x04 To clear interrupt flag write to register,value 0x02, 0x0F */