Hi Steven,
thank you for your feedback, I created a new thread.
Challenge:
We want to generate very short LED pulses (1µs or better 0.5µs) with high current (minimum 2A, better 3A) that can be controlled (dimmed).
The pulses should be adjustable with a frequency between 30 and 200Hz. Input voltage is probably around 24V but could be changed if needed. We want to drive 1 to 4 LEDs with each 3V to 3.6V drop.
Can we do this with the TPS92641 and how do we need to configure it? Is there a dev board for testing?
Thank you very much!