Other Parts Discussed in Thread: TPS65987
We have developed a board with the TPS65987, and want to support two modes of operation, that should be user selectable.
The user should be able to select between to modes "new" and "retro".
In "new" mode, the devices attached should be able to negotiate 5-20V, we have used the configurator program and created an image for this, which works when loaded into the spi flash on our board.
In "retro" mode, the devices attached should only get 5V, we also have an working image for this.
We have an MCU connected via I2C, but it seems as a rather big project, to download the images, using i2c interface, and they would also take up a lot of flash in the mcu.
Is there any way to do this without downloading an entire image, when switching between modes ?
Can we as an example, just have the TPS65987 switch between two images in the spi flash ?
Or how is this done.
Best regards
Jakob