This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: SPMI no clock after power up at high temp

Part Number: TPS6594-Q1

Dear expert,

1. Air temp 80C, Tj 110C~120C, TPS65941213Q1 SPMI abnormal after power up result lose communication with LP8764. 100% reproducible at high temp.
2. One pcs TPS65941213Q1 among 15Ku report this issue.
3. No any voltage output. Register report SPMI abnormal. There are only 8 SPMI clock after power up then no signal. Scope capture is at next page
4. ABA swap experiments, problem goes with this pcs TPS65941213Q1

Scope capture is in attached PPT.

Is there any suggestion before I send to CQE process?

Thanks

TPS65941213PWERQ1hightemp_SPMIissue.pptx