Hi TIs,
I have design-in with TPS61199PWP model, .
So , i have some question need TIs help yo clarify
1. How do I know that when I change the PWM, the current will change according to the PWM duty. If I change the PWM to the next level, how long will it take? Is it 1μsec?
2. If I continuously change the PWM duty, will it be affected? have time or specification define to this?
3. If the current required by the load is 280mA (IFB 1 to IFB 6), and my ISET setting is 40.5mA, is this value too small?
My environment:
VIN input voltage : 12V
Vout voltage : LCD Panel ( VDD = 19V to 26V , ILED=280mA )
Thank you
Rai.