This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: charging current is very less

Part Number: BQ25792
Other Parts Discussed in Thread: BQ25798, , BQ25790

Hello Ti,
I am using BQ27292, keeping Registance value 50K between REGN (pin 5) and ILIM_HIZ (pin 17), 100K between ILIM_HIZ (pin 17) and GND.

the charging current is very less and i.e. 0.8A at 5V from VMAIN+. (Battery configuration 2 parallel battery of 4500mAH).

for reference please find the attached schematic. (as footprint are same we are using BQ25792 instead of BQ25798)


Regards,
Abhineet Ranjan