This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B86-Q1: TPS7B86-Q1_LDO Pspice Model

Part Number: TPS7B86-Q1

Hello Nick,

Thanks for your feedback !!

We want to understand the device and PG pin behavior when Vout gets short to BAT voltage for different Vin i.e. 8V,13.5V,18V & 24V. 

Whether the IC will have no impact in the above-mentioned scenarios?

As mentioned in your last comment you expect PG pin to be pulled down low once the Vout is above its sets point i.e 5V in our case considering MPN : TPS7B8650DQDDARQ1 , Can you check & let us know whether the PG pin remain pulled down low in case Vout gets short to Vin when Vin= 8V,13.5V,18V,24V.

Considering above mentioned point Please let know the PG pin state(High/Low) at different voltages when Vin is increased in step of 1V from 0V to 24V. 

Please check if your team can prepare the pspice model with PG pin as well parallely.

  • Hi Shersingh,

    I can test the short to battery conditions in the lab when I'm in tomorrow. Is this device used off-battery such that the input voltage is equal to the BAT voltage during these short conditions?

    Considering above mentioned point Please let know the PG pin state(High/Low) at different voltages when Vin is increased in step of 1V from 0V to 24V.

    Is this a separate test than the above mentioned test or an extension of it? ls the BAT voltage constant while VIN is swept or is VIN = VBAT?

    Our team does not have the resources to prioritize this model creation at the moment. 

    Regards,

    Nick

  • 1. It is an extension of it as we need to check for our complete operating voltage range of the system i.e 6V to 24V.

    2. Please perform the required test at your end and let know the LDO behavior and PG pin status in all the condition mentioned in the thread above - Awaiting for the test results. 

  • Hi Shersingh,

    I still do not have a complete picture of the tests you are requesting. Can you please address all of the questions in my last comment?

    Thanks,

    Nick

  • Hi Nick,

    I had already addressed all of the questions in my above comment!! Pl let know if you any query is unaddressed.

    Any update on the testing results? 

    Are our raised request for testing the LDO behavior is so time consuming as it has been pending since an week.

    Could you pl expedite and share the required results.

  • Shersingh,

    Is this device used off-battery such that the input voltage is equal to the BAT voltage during these short conditions?
    ls the BAT voltage constant while VIN is swept or is VIN = VBAT?

    I need to know the answer to these questions because it is not clear to me whether a short-to-battery in this case means that the VIN of the LDO is equal to the battery voltage. In some applications a short-to-battery is the same as VOUT = VIN, and in some cases the VBAT > VIN so that when there is a short-to-battery condition, VOUT > VIN. 

    If a week is too long for support, I advise following up in time intervals that are less than 5 days. 

    Regards,

    Nick

  • Hi Nick,

    In our case Vin=VBat and we need the results for the LDO behavior and PG pin status when Vout is gets short to Battery voltage which may be in the mentioned range of 6V to 24V. 

    Above results can be captured on Vin of 6V,8V,13.5V,18V & 24V. 

    Thanks for your support , We were expecting some progress in an week time.

    Please check if you can manage one of the resource who can work on development of Pspice model as well with PG pin.

  • Hi Shersingh,

    I am getting this set up on an EVM. I will finish up tomorrow and send you the results. 

    Thanks for your support , We were expecting some progress in an week time.

    If I had all of the information I requested I could have finished this in one day. Next time, please be sure to follow up with the requested information before your time frame has already passed. 

    Regards,

    Nick

  • Thanks a lot for your help & support!!

    The required condition to be tested was already discussed in detail for 13.5V condition with Umesh who initiated this thread.

    I don't know why Umesh did not had a discussion internally in the meantime with you.

    Pl check if you can arrange the Pspice model of it with PG pin by managing your resources in upcoming days, that will be really helpful to each of us and other customers as well.

  • Hi Shersingh,

    The PG functionality is not as I expected; it acts like a Schmitt trigger, so when the output goes above its set point during a short-to-battery event, the PG pin remains high impedance. I tested this up to 18V because PG is only rated to 18V. In summary: when the output is shorted to voltages less than about 4.55V, PG is pulled low, and when the output is shorted to voltages greater than about 4.55V, PG is pulled high. 

    We are understaffed right now, and it would be me that would handle the creation of a new PSPICE model for you. I am telling you that we as a team and I as an individual contributor do not have the resources for this right now. 

    Regards,

    Nick

  • Hi Nick,

    Could you please share the readings / graphs of pins Out, FB/NC pin when EN=1 and Vin is increased in step of 0.5V or 1V for the range 6V to 24V.

    Please perform the above-mentioned test above 18V as well, please check whether it is leading to any failures to the LDO.

    What will be your plan if we need the Pspice Model with PG pin considering the available resources at your end - Can we have any tentative date for it as our end customer need the simulation results as well. 

    Thanks a lot for your support!!

  • Hi Shersingh,

    Could you please share the readings / graphs of pins Out, FB/NC pin when EN=1

    This is a fixed device so I could not probe FB/NC, and EN = 1V does not result in the device being on as the minimum ON state is 2V, so that is what I used. See the results below. 

    As I mentioned in the last slide, the PG pin did not seem to be damaged by the 24V that was seen on it, but that does not mean the customer should do it because this was one unit tested at room temperature so there is no guarantee that devices will not be damaged by this and they should still comply with the abs max ratings. 

    STB Test Results.pptx

    I can talk to my management to see what we can do about the PSPICE model. This will take a lot of effort so I wouldn't expect to have any model to share before August at least. 

    Regards,

    Nick

  • Hi Nick,

    Thanks for sharing the test results !!!

    Please have a discussion with your management and initiate the actions for the required Spice model.

    We will be waiting to hear from you regarding the PSpice model progress post your discussion with the management. 

  • Hi Shersingh,

    I discussed this with management and they are of the same opinion in that we do not have the resources to publish a new model right now. It will for sure be a 2H release window. If there is another way we can help to support your customer's needs let us know.

    Regards,

    Nick

  • Hi Nick,

    I already had a discussion with the customer in past, they are very clear to have the Pspice model for the simulation and ready to wait till Month of Aug as proposed from your end.

    So kindly initiate the tasks for the Pspice model accordingly considering its deliverables.

  • Hi Shersingh,

    August is a tentative date. We will do our best to deliver it by then.

    Regards,

    Nick

  • Hi Nick,

    We have good hopes from TI for their deliveries. 

    Could you please share the circuit details which was tested for the range of 6V to 24V? which is not included in the shared presentation.

  • Hi Shersingh,

    Sorry about that, the PG pullup resistor was 10kΩ, C_DELAY = 1uF, and CIN=COUT=2.2uF. 

    Regards,

    Nick