This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We want to use TPS3760 supervisor IC in our project. In specific, we want to use TPS3760B302DYYR-Q1 and TPS3760BA22DYYR-Q1. But these two are not available to buy. Where can we buy these two specific ICs? What is the other solution if we couldn't buy these?
Hi Akshay,
As you have stated these variants are not available for purchase. Could you please explain the necessity for a push-pull device? Our TPS3760A012DYYRQ1 is an open drain active low IC that has adjustable threshold to meet both your desired 3.0V and 11.2V thresholds. Will both of these devices be used within the same project? If you could, please share a block diagram or schematic.
Thanks,
Joshua