Part Number: UCC12050
I am configuring a circuit using UCC12050DVER as shown in the attached document.
As shown below, it seems that the behavior is not in accordance with the specifications.
(1) According to the specifications of UCC12050DVER, if pin 13 (SEL) and pin 14 (VISO) are shorted, 5.0V should be output in theory, but when measured, only 3.38V is output.
(2)According to the specifications of UCC12050DVER, the current flowing to VINP should theoretically be about 50mA when there is no load, but when measured, it was 192mA.
What I would like to ask you is
・Could you please point out if there is anything wrong with the circuit configuration?
・Since it was purchased from a mail order site, there is a possibility that the parts may be defective. Is it possible to determine that there is a failure based on the events ①②③④ in the attached document?