Good morning, following the guide in the bq24610 datasheet, I arrived at this circuit with these values. Regardless of whether the configurations are correct or not, I calculated a VBAT of 11.1 because I will be using 3 batteries of 3.7V in series. My question is whether charging the batteries in series as shown in the diagram is correct.
Note: I will power the bq24610 with 5V