Other Parts Discussed in Thread: TPS25730, TPS25730EVM, , USB-PD-CHG-EVM-01, BQ25731, BQ25792, TPS25751
Hi
I am facing the same problems as described in this 2 year old case. The GATE voltage is not high enough to turn on the NFET. The TPS25750S is configured as a power source. The correct PDO with 9V has been negotiated between the PD source and the sink (TPS25730). I can see that the GATE voltage is lifted from 0 to approximately 5V, but as the VSYS bus is 9V the GATE voltage most be at least 10V for the FET to turn on. The GATE is held at 5V for approximately 1s, and then returns to almost 0V. VBUS drops to 0V during this proses and as a result the sink device gets restarted, and the proses starts all over in an endless loop.
I use the MIKROE-5682 module from MIKROE as the test platform for testing the TPS25750S,and the TPS25730EVM for the sink. VSYS is powered with 9V. I have a MCU connected to the I2C bus and can read the registers in the TPS25750.
Any idea of how to fix this?