May I know what is the switching frequency of the internal Buck-Boost converter? Thanks
BR,
Gary
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
May I know what is the switching frequency of the internal Buck-Boost converter? Thanks
BR,
Gary
Hi Gary,
The buck boost converter doesn't have a set frequency. It restarts the switching cycle once the current in the inductor hits 0A. So the rise time and fall time of the inductor current is affected by the inductor value used. For a 22uH we see ~500kHz switching frequency, you can scale this to a 10uH inductor which should be ~1.1MHz.
Best,
Kyle Wolf