This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23523: function of TMR ,ICL and ICL2

Part Number: TPS23523

Hi,

In the example calculation in the datasheet, I saw the time out of the TMR(2ms) is less than the soft start time().

*What is the function of a TMR?, at what time does the timer time out?

*Does the selection of hot-swap mosfet depend on ICL and ICL2,or is it just the max Cout current?

*The inrush current margin datasheet states 0.4A. Is it possible to increase the value?

Thanks, regards,

Anoop