Other Parts Discussed in Thread: USB2ANY, IPG-UI, TIDA-00606
Hi,
We are facing communication issue with IPGUI to TPS65218EVM-100, So as we turn ON EVM kit with input VSYS (5V/3A) we are getting the default outputs which mentioned in datasheet, but we are not able to reprogram or read/write the registers DCDC1-DCDC4 & LDO1 via I2C Communication using USB2ANY. We are suspecting that I2C communication is not working here also we have checked the frequency in SCL and SDA line with DSO No frequency was captured except pull up value 3.3V. Kindly help on this issue, Expecting response as soon as possible.
Thanks,
Yashar