This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5450-EP: SMPS Output volatge set

Part Number: TPS5450-EP

Hello 

I am using TPS5450DDA in my project.

Input-28VDC

Output- 5V/5A

I have done above voltage with current.

1. Can I adjust output voltage 6.3V/5A  with 28VDC input.

2. Who much adjust output voltage