Other Parts Discussed in Thread: DRV8833
Dear TI,
I have a baffling situation that I don't fully understand where I did wrong of I have failed to consider. At the moment, I have a TPS61178 with LI-PO (3.7-4.1V) as input and my output is 5V.
I use this boost converter to drive a motor driver DRV8833 also from TI. The motor driver connects to two stepper motors in parallel (front and rear motors) since I want the two motors to run sychronized and reduced footprint.
I have tested and confirmed that the DRV8833 can drive two stepper motors in parallel with bench-top supply as input. However, the TPS61178 has significantly voltage drops at output (no longer regulating at 5V but 3.7 V instead).
I tested the TPS61178 with a constant load 8.6 Ohm resistor and, and I saw that the output voltage remains steady at 5V, resulting 580 mA of current output.
here is the Schematics and I am curious what you think. Please ignore the radio module. Only the TPS61178, the antagonistic valve uC, and the valve driver are installed.
Thank you very much and I look forward to hearing from you
Khoi