Other Parts Discussed in Thread: UCC28180, , UCC24624
We are currently working on 750W desing in which we have use UCC28180+UCC256404+UCC24624 IC combination.
In which at initial start up there is a current spike in resonant as you can se in below image. Which is around 22A peak to peak. Sometimes it also goes in OCP, and unit is start after two to three hiccups..
Pink is resonant current
Green is Boost voltage
Yellow is RVCC

Could you please suggest us in which section we need to work or do modification to reduce this spike.