This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Built boards with the circuit in the linked forum post.
However, I'm not seeing any output voltage. It's supposed to be -14.6V. We disconnected any output circuitry to isolate the issue. EN pin (pin 5) is 1.300mV, and VIN (pin 3) is 5V. I probed the SW signal (pin 2) and am not seeing any oscillations.
The EN pin is going through a voltage divider of 22k over 7.63k with the top attached to 5V and bottom attached to the -17V rail. So it should be 5.66V above the -17V rail, well within the 7Vmax,EN.
Inductor is 56uH, and feedback network is 47k over 2k with 100pF (compensation as per Webench) from Vfb to the output of the inductor (GND).
Thanks,
Derek
Hi Derek
Can you please attach your updated schematic?
Before the device start up, the '-17V' hasn't start to build up, the IC_GND is 0V same as system GND. So when 5V Vin is applied, the EN to IC_GND voltage is 5V*(7.63k)/(22k+7.63k) =1.28V, which is quite near to the V(EN_RISING) specified in the datasheet. Please configure the voltage divider so that the EN to IC_GND is higher than 1.35V to make sure the device can normally start up.
After the '-17V' build up, the the EN to IC_GND voltage is (5+17)V*(7.63k)/(22k+7.63k), and you are right we need to keep this value <7V.
I am not sure how comes the EN pin (pin 5) is 1.300mV, can you please check about this?
Thanks and best regards.
Schematic is below. I originally tried it with the EN resistor divider of 100k over 7.87k but that didn't work either. What's the best way to ensure that the EN pin is > 1.35V above IC_GND (in this case our -17V rail) but doesn't exceed the VEN,max of 7V? If the resistor divider is 22k over 10k then:
startup: VEN = (10k/32k * 5V) = 1.56V above IC_GND
running: VEN = 10k/32k * (5V + 17V) = 6.875 above IC_GND
That would work, but without very much margin on either side. I guess another way to do it (although sloppy) would be to hit it harder (e.g. a resistor divider of 10k over 10k) so that while running the output of the resistor divider is higher, but then use a 5.6V zener from EN pin to IC_GND to restrict that voltage to 5.6V above IC_GND.
I re-measured VEN. With the current resistor divider (22k over 7.87k) it is measuring 1.27V which makes sense because (7.87 / (22 + 7.87)) * 5V = 1.3V.
I also overnighted a replacement TPS54202 in case this one was damaged. I also have other boards I can test.
Thanks,
Derek
Hi Derek
I the 22k over 10k solution can work. If you want to leave more margin and the power dissipation on the Zener wouldn't be a problem, you can add a Zener diode between EN and IC_GND.
Does the circuit operate normally now?
Thanks and best regards.
Hello, I changed the resistor divider to 22k over 10k and also replaced the IC and it is working now. Thank you.