This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2660: max output current of LM2660M

Part Number: LM2660

The customer want to know the max output current of LM2660. (Output power capability)

In the datasheet, the output current Min is 100mA.

The Maximum V+ and out continuous output current is 120mA.

How can we understand the above two parameters?