This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25924: RT1720 replacement

Part Number: TPS25924


Hi Team

do we have any other replacement for RT1720?

customer side need automotive version

BRs

Brian

  • Hi Brian,

    Do they need an integrated solution or hot-swap solution? Can you explain how the customer is using RT1720.

    I am adding some of the features of RT1720 from there website.

    • Wide Input Operation Range: 5V to 80V
    • Negative Input Voltage Rating to −60V
    • Adjustable Output Clamp Voltage
    • Adjustable Over-Current Protection
    • Programmable Timer for Fault Protection
    • Low Shut Down Current
    • Internal Charge Pump N-MOSFET Drive
    • Fast 80mA MOSFET Shut-off for Overvoltage.
    • Fault Output Indication

    Can you tell me which feature is very critical in their application. Like voltage range or negative input voltage rating? etc. 

    I am also assigning this thread to my colleague who handles high voltage eFuse. 

    Best Regards,
    Arush

  • Hi Brian,

    As we had our discussion directly, I am closing this thread. Please click on resolved to close it from your end also.

    Best Regards,
    Arush

  • Hi Arush

    Many thanks for your help Slight smile

    BRs

    Brian