This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24296M: Precharge and termination current settings

Part Number: BQ24296M

Hi.

The defaults for this IC are IPRECHG = 128 mA and ITERM = 256 mA.

Is setting the same value (e.g. both 128 mA) for the precharge and termination currents okay? No negative effects or special behavior with IC's state machine, which must be treated on top of default methods (like for REG02[0] bit)?

Regards, Vasyl.