This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z746: about StateofCharge rises or down

Part Number: BQ27Z746

Hi Titeam


We have a project on lithium iron phosphate; After being fully charged, the SOC is 100%, and when placed, it will automatically drop to around 90%; How can I avoid not falling down? I also tried to turn off the SMOOTH function, but it was still the same;
Charging to around 80%, it also automatically rises when placed.;Abnormal log data 1.zip6136.gg.csv