This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS4811-Q1: What is the maximum switching frequency?

Part Number: TPS4811-Q1

Hi TI Team,

I'm using the TPS48110 in my new project. In this project, I need to switch a solenoid load at a specific switching frequency. For this application, I have selected a MOSFET with a total gate charge of 20nC to drive my solenoid. I have included a Gate turn on resistor of 10 ohms. The maximum allowable turn-on time of the MOSFET is 2% to 5% of the maximum switching frequency. Also, I cannot use a separate auxiliary voltage; this should operate from the internal charge pump only.

Additionally I can keep Bootstrap capacitor in the range of 2nF to 10nF. Kindly let me know the max. switching frequency that I can operate with this considerations.

Kindly reply as early as possible.

Thanks in advance!