This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24618: Reliability issues

Part Number: BQ24618

Hi,

This is related to my previous question regarding BQ24618 as I have been looking into the design again.

The BQ24618 circuit is part of a larger charger design which has had two versions. The circuit I shared previously is almost identical between the two versions, the major change being the input to the circuit: Version 1 had no reliability issues and used a conventional DC adapter, whereas version 2 uses USB PD. Both provide 20V, however the USB-C has a slower rise time (~150us vs ~25ms).

Does BQ24618 have any requirements regarding input voltage ramp up time? Could the slower rise in the second version cause these random failures and is it worthwhile to implement a separate enable circuit?

Thank you for your help!

  • Hello Boris,

    Does BQ24618 have any requirements regarding input voltage ramp up time? Could the slower rise in the second version cause these random failures and is it worthwhile to implement a separate enable circuit?

    We don't have a requirement for input voltage ramp up time, this is not something that we test, so I can't confirm if this is what caused the reliability issue. However based on the information given, I do think this could be a possibility and adding the separate enable circuit could fix the issue.

    Best Regards,

    Christian.