Other Parts Discussed in Thread: LM5175
We have made some prototype PCBAs using the LM5176 based off the reference design and the circuit is operational but showing high quiescent current draw of ~150 mA at no load. The current consumption is consistently ~150-180 mA across a 9V-48V input range. This is causing excessive power dissipation in the inductor which is concerning for our application. I can see on the thermal camera that the inductor is reaching ~60C.
Here are photos showing it on a DC load at 0 amps and 100 mA load. At 0 mA load the system is consuming 150 mA at 12.8V (4.5W).
I can verify the downstream system is only drawing 10 mA @ 24V input by applying a separate power supply to the V_SYS rail bypassing the LM5176, so I don't believe the loss is in our system.
Is this a control loop issue? A component selection issue?
Please find the attached design spreadsheet and schematic and let me know if you see any issues. I'm happy to collect more data as needed too.
Thanks!
-Mike