On a new design we're working on, we are currently experiencing the same issue as described in this post:
Configuration Question to Support USB2 Network Adapter
The issue is that a phone will not recognize a connected USB device when the 762-Q1 is charging the phone. After some debugging, we suspect the lack of a USB-PD "role swap" is the root of the issue that's preventing the phone from seeing the connected USB device when the 762-Q1 is charging the phone.
Questions:
1. Have there been any updates in the 762-Q1firmware, that allows the device to do a USB-PD "role swap"?
2. Are there plans to add this feature to the 762-Q1 at some point in the future?
Thanks