Other Parts Discussed in Thread: TPS61023, TPS61022
Hello:
Please confirm if the maximum pulling current of 1.4ATPS612592YFFR meets the requirements?Thanks!!!
Turn on the reverse wireless switch (just turn on the switch, do not perform reverse wireless charging), use an electronic load meter to load at the output end of the circuit, step by 100mA to increase the current on the electronic load. When it reaches a certain critical value, the output voltage on the oscilloscope drops to 0 or the output current drops to 0. At this time, the upper limit of the inductor current is the overcurrent protection point current value.
Actual measurement result: The electronic load meter draws BOOST-OUT to 1.4A, and at this time, the inductance (PL4001) current is 3.05A, triggering OCP.