Hello,
regarding the circuit solution proposed in the datasheet for Reverse Input Voltage Protection With IQ Reduction:
Diode D3 has Average Rectified Forward Current = 1A and MOSFET Q2 has (Max) Continuous Drain Current = 2.2A.
I ask, is it not enough to use, for example, a diode with Average Rectified Forward Current ≈ 0.25-0.3A and a MOSFET with (Max) Continuous Drain Current ≈ 0.17-0.2A?