Part Number: BQ24253
Other Parts Discussed in Thread: BQ25616
Hi support team,
I have two questions about the D± pins.
Regards,
Dice-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dice-K,
Please see my answers to your questions below.
1) Yes it is recommended to isolate the connection of D+/D- lines to either BQ24253 or MSP430 using a multiplexer, etc. Once BC1.2 detection is complete the /PG pin status on the BQ24253 will change. This signal can be used to change the D+/D- connection to the MSP430 for data transfer.
2) If D+/D- based detection will not be used I recommend shorting D+/D- pins together. Shorting the pins together will result in DCP detection and then current limit is set by ILIM resistor.
Additionally, I wanted to bring your attention to a newer standalone charger option the BQ25616. This part has similar features to the BQ24253 and is years newer and lower cost.
Best Regards,
Garrett