This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Please tell me a few things.
1, The AltManufacturerAccess() register has two different command numbers, 0x00/0x01 and 0x3E/0x3F, and the former overlaps with the Control() register.
Which one should I use or how should I use them differently?
2, There are also two different notations, AltManufacturerAccess() and ManufacturerAccessControl()[0x3E/0x3F], as shown below.
If the command numbers are the same, including the Control() register, are the functions the same even if the names are different?
Sincerely,
Ryu.
Hi Ryu,
1)
2) I am unsure what you are referring to when you say AltManufacturerAccess(), what documentation are you referring to?
Regards,
Evan
Hi Evan,
It is described in 7.3.8.2 of the data sheet.
It is noted that the same number is written in 7.3.8.2 and 7.3.8.3.
Sincerely,
Ryu.
Hi Ryu,
Thanks for pointing that out.
Control, MAC, and AltManufacturerAccess are all very similar. MAC and Control function the same way while AltManufacturerAccess is used to read/write entire blocks of data rather than a single parameter.
Regards,
Evan
Hi Evan,
Does AltManufacturerAccess() exist in the q35100?
There is a description of AltManufacturerAccess() in section 7.3.8.2 of the bq35100 datasheet, but it is not present in the TRM.
I checked if there is a description of AltManufacturerAccess() in the TRM of bq28z610-R1.
As a result, there was a description.
Therefore, if there is no description in the TRM of bq35100, does it mean that AltManufacturerAccess() does not exist in bq35100?
Sincerely,
Ryu.