Other Parts Discussed in Thread: BQSTUDIO
Hi,
I have a design using the BQ76952 that I've been working with Luis on. The prototype came in and everything seems to be working fine but we are seeing two odd issues.
1. With the a 4S of batteries which is about 15V in our system and nothing connected to the PACK, we are reading the pack voltage at 16.5V and sometimes even higher via the ADC in the BQ76952. When we measure it with a voltmeter, the voltage snaps back to 15V. How can this be happening?
2. CELLs 0-2 when reading the voltages in bqStudio seem to be right on. I'm measuring then with a voltage meter as well. But the ADC reading of the CELL16 is much higher than the actual cell. The cell is about 3.9V but we are reading close to 4.3V via software. We did change the series resistor on Cell 16 from 100 ohms to 20 ohms which was suggested by TI since it powers the Cell balancing but this is really the only difference between CELL0-2 and CELL16 between the batteries and the BQ76952. Is their a reason for this?
Thanks!!!
John