We are using Schematic as
TPS53667EVM-769
we can read IC addresss , but NO PWM ouput from TPS53667 ,if you have the experience
please Let me know to do ?
THS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Luo,
Our team will get back to you on this.
Best Regards,
Dhanya Prem
Hi Luo,
Could you please provide more information in your case?
1. Did you power on the system both following the sequence for 5V/3.3V with controller and SPS?
Please following the 7.1 Test Procedure in the TPS53667 EVM User Guide.
2. Please check the fault status with Fusion GUI if there is still no output voltage.
Best regards,
Jack Su
Hi Luo,
It seems that the power on is failed because of OVF.
Could you please check VIN to VOUT and VIN to SW//per-phase with meter in Ohm mode?
And confirm GND to VIN/VOUT/VCC/VDD/SW if there is any short circuit issue.
I believed that is a root cause!
Best regards,
Jack Su
Hi Luo,
Could you please send Project File.xml and Schematic File to me jack_su@ti.com for reviewing the configs setting?
Thanks!
Best regards,
Jack Su